Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: ENERGIA
Tool/software: Code Composer Studio
Hellow everybody,
I have made a CCS program for control a buck converter that basically reads with the ADC the output value of the voltage and modulate the PWM in order to fit it to the selected value. Now I would like to improve it and do it from my browser with a simple CGI program. I have worked beafore with Energia to build up this kind of CGI project using the ethernet library and the server and client class, so I was able to show the web pages i create in html and capture different information that the users introduced. The problem is that I hardly find examples of how to make this with CCS projects, and those examples that I find, such as enet.io, where impossible for me to understand, so if please anyone could gave me a more simple example of that or explain me how to add ethermnet class to CCS projects I would be forever thankfull.