Part Number: TMS570LS1227
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hello,
I'm wanting to use SCI to write to and read from a TM570ls1227PGE using the PuTTy terminal emulator. To do this, I enabled both the SCI RX and TX interrupts in halcogen, but am only receiving a single byte of a string when I attempt to sciSend in CCS. However, when I disable the TX interrupt, sciSend performs normally.
I'm assuming that this is because SCI is interrupting the RX process to do a TX "handshake" when I have that interrupt enabled. Is that the case?
As well, is the idea of using a single sciREG to send info to the terminal and write from the terminal even possible?
Thank you!