The CAN of TMS470mf0660x is Very, very difficult to use,TI should provide some example code about the CAN module,but where could find the example code?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please find the attached TMS470M_DCAN_Sample_Code a CCS3.3 based pjt file, to use it in CCS4 use option "import legacy CCS3.3 pjt."
This is a simple pjt file in which CAN1 communicates with CAN2, you can use this to understand the basic module configuration and useage.
Note: TI is planning to release a Code generator tool soon for TMS470M series of device. This will be a GUI based tool, which can be used to generate basic driver files with a click of a button.
Best Regards
Prathap
Dear Prathap-san,
You write as the following.
> This is a simple pjt file in which CAN1 communicates with CAN2, you can use this to understand the basic module configuration and useage.
Please describe more detail for this project. I would like to show our customer CAN communication demo with TMS470M. But I am beginner for
CAN communication.
Best regards,
Michi