Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Hello,
I have an RM48 HDK, Iam programming in Keil uVision5 RTX-RTOS, and I am using a Seeger JLink programmer. I have written the simple example program below. After calls to os_dly_wait() in both tasks , the console reports "* JLink Info: Memory access: CPU temp. halted: https://wiki.segger.com/Memory_accesses#Stop_mode," and the program stops.
#include <RTL.h> /* RTX kernel functions & defines */
#include "rti.h"
#include <stdint.h>
volatile U32 g_os_err_code;
/* id1, id2 will contain task identifications at run-time */
OS_TID id1, id2;
int counter1;
int counter2;
/* Forward reference */
__task void task1(void);
__task void task2(void);
/* Used for debugging */
uint32_t sys_time;
__task void task1(void)
{
/* Obtain own system task identification number */
id1 = os_tsk_self ();
/* Assign system identification number of task 1 to id1 */
id2 = os_tsk_create(task2, 1);
while(1)
{
sys_time = os_time_get();
counter1++;
/* Indicate to task2 completion of do-this */
os_evt_set (0x0004, id2);
/* Wait for completion of do-that (0xffff means no time-out)*/
os_evt_wait_or (0x0004, 0xffff);
/* Wait now for 50 ms */
os_dly_wait((uint16_t)5);
sys_time = os_time_get();
}
}
__task void task2(void)
{
while(1)
{
sys_time = os_time_get();
counter2++;
/* Wait for completion of do-this (0xffff means no time-out) */
os_evt_wait_or (0x0004, 0xffff); /* do-that */
/* Pause for 20 ms until signaling event to task1 */
os_dly_wait((uint16_t)2);
/* Indicate to task1 completion of do-that */
os_evt_set (0x0004, id1);
}
}
int main(void)
{
// Enable interrrupts.
__enable_fiq();
__enable_irq();
os_sys_init(task1);
}