Part Number: TMS570LS3137
Hello Team,
My customer is connecting TMS570LS3137 to an ethernet switch IC (Microchip - KSZ8775). This switch provides either MDIO or SPI interface using the same pins. The MDIO interface on the switch allows for access to the PHY, while SPI allows full access to all the registers on the switch.
Would it be possible to disable the MDIO on the TMS570LS3137 (use as GIOs) since the customer has SPI into the software?
Any feedback you can provide would be appreciated.
Thanks,
Sem