Part Number: EK-TM4C1294XL
Hi, I'm trying to use the UART5 receive interruption with my tm4c1294xl launchpad board but I'm getting stuck because the ISR is not being called, bellow is my code
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "driverlib/gpio.h"
/*variable to keep system clock*/
uint32_t g_ui32SysClock;
void init_serial(uint32_t system_clock, void (*pfnHandler) (void)){
/*Enabling Peripherals*/
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART5);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
/*Setting Up pins*/
GPIOPinConfigure(GPIO_PC6_U5RX);
GPIOPinConfigure(GPIO_PC7_U5TX);
GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);
/*UART Configurations*/
UARTConfigSetExpClk(UART5_BASE,system_clock,115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
/*Enable uart interruptions*/
IntEnable(INT_UART5);
UARTIntEnable(UART5_BASE, (UART_INT_RX | UART_INT_RT));
/*Registering UART isr*/
IntRegister(INT_UART5, pfnHandler);
}
/*ISR for uart5 receive or receive timeout interruption */
void UARTIntHandler(void)
{
uint32_t ui32Status;
//
// Get the interrrupt status.
//
ui32Status = UARTIntStatus(UART5_BASE, true);
//
// Clear the asserted interrupts.
//
UARTIntClear(UART5_BASE, ui32Status);
//
// Loop while there are characters in the receive FIFO.
//
while(UARTCharsAvail(UART5_BASE))
{
//
// Read the next character from the UART and write it back to the UART.
//
UARTCharPutNonBlocking(UART5_BASE, UARTCharGetNonBlocking(UART5_BASE));
//
// Blink the LED to show a character transfer is occuring.
//
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
//
// Delay for 1 millisecond. Each SysCtlDelay is about 3 clocks.
//
SysCtlDelay(g_ui32SysClock / (1000 * 3));
//
// Turn off the LED
//
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
}
}
int main(void){
/* Set the clocking to run at 120MHz */
g_ui32SysClock= SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
/*Start string*/
uint8_t *cThisChar = "Starting...";
/*Onboard led just for verifications*/
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0x00);
/*Enabling processor interrupts*/
IntMasterEnable();
/*serial configurations*/
init_serial(g_ui32SysClock, UARTIntHandler);
/*Sending initial string*/
while(*cThisChar != '\0'){
UARTCharPutNonBlocking(UART5_BASE, *cThisChar++);
}
while(1){
/*Wait interruptions*/
}
/*no errors*/
return 0;
}
Code is compling with no errors but when I send something to the board the receive interruption is not triggered.