I find that the tm4c129encpdt on the board which the client sent back became green as below。 can somebody tell me why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I find that the tm4c129encpdt on the board which the client sent back became green as below。 can somebody tell me why?
B.P. (just) may have 'broken new ground' w/this one!
Are the MCU pins (really) gold plated?
And - if that's so - is not gold (deliberately chosen) as it superbly resists 'oxidation/corrosion?'
Copper is 'known' to 'turn green' due to simple oxidation. It is highly likely that (some) contaminate (possibly an 'imperfect' soldering or board-cleaning process) has produced this effect. Staff's 'eagle eye' detects that this MCU appears to have been 'removed' from its assembled pcb - which 'removes' the ADDED CLUES - which such BOARD EXAMINATION (not just a single chip) would provide! (i.e. how far did this contamination/oxidation physically 'spread' - what else & other areas - were impacted?
No report of board/device performance arrived - nor of the 'operating environment' (sub-surface, marine use - perhaps?) That's of (some) consequence - is it not?
Chip and/or Board Assembly ABUSE - or subject to severe moisture-laden environment (while improperly protected) (i.e. encapsulant-free) all may trump (other) explanations...
As listed in Appendix A of the datasheet, the leads are copper with Nickle, Paladium and Gold layers on top (CU NIPDAU). As CB1 mentioned, copper will oxidize green. From the picture I cannot determine if the green color is oxidized copper or a containment left on the leads from solder flux or something else. As Danny F mentioned, knowing what happened to the parts might help, (storage, age, solder process, removal process). Why do yu ask? Was there a continuity problem before the devices were removed from the board? Here is the plating depth of different metals:
BP101 said:There be white gold on them there pins
Was not that phrase, 'Gold in them 'thar' hills (or now, pins)? (we need to insure 'accuracy' of our historical references - do we not?
Your 'leaky electrolytic' (or similar) registers as 'far more likely' than (earlier) - 'multi-legged, fast/shifty, escape-artist' creatures.
The curious wording, 'MCU becomes green' - seems to suggest that the MCU - uniquely and 'on its own' (i.e. without (any) external influence) - became so corroded.
When posters provide the bare minimum of data - especially when omitting the 'particularly vital' (i.e. the 'rest of the pcb') - my suspicions (naturally) rise! (Why go thru the trouble of 'removing the MCU?' ... What if that 'green-plague' - extended far beyond 'just' the MCU? ... Might that be of great 'inconvenience' - to the 'failed MCU claim?)
Improper - possibly (even) acid-based solder flux - or board 'cleaner' - or some 'after assembly assault' - rapidly climbs - this 'green-tinged', Suspect List!
Your first link is 'dead' ... second provides NO INDICATION of the, 'Cause of pin corrosion.' (JTAG issue (only) is described - which bears NO RELATION whatsoever - to MCU corrosion!)
Many questions were asked regarding your board's handling - operating environment - and 'correctness of processing & assembly.' Not one was answered - that's 'telling' - is it not?
No one here can (ever) recall vendor's MCU suffering such fate - by itself - when handled & processed properly. As the vendor agent noted (in his reply) ... 'what happened to your parts?' ... minus that KEY INFO - your posting has little chance of being understood - even less ... of being resolved...