Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Team,
I am posting on behalf of my customer as this is urgent:
In our project we are severely struggling with computing performance of RM48L952. After inspection, it seems that the bottlenecks are in over-EMIF access to the external SDRAM and to the internal code FLASH. What are the things that we should pay attention to get the potential performance realized on these interfaces?
Additional info/questions received in the meantime:
After inspection it seems that the bottlenecks are in the over EMIF access to the external SDRAM. According to our tests the reading of SDRAM is about 10-times slower than from internal RAM and the writing is 2-times slower (test code attached).
SDRAM: ISSI IS42S16800
Processor: RM48L952, silicon rev D
Open questions:
- Is it possible to run SDRAM at higher frequency than 55MHz?
- According to the user documentation: “normal memory type” mode (NORMAL_OINC_SHARED) speeds up the interface – is it possible to configure silicon rev D to this mode with SDRAM?
- Memory conf attached. Is there something that could be done to improve the performance?
Best regards,
Frank