Other Parts Discussed in Thread: RM48L952
Hello there,
We would like to use the CPU2A and CPU2B diagnostics (Boot Time and Periodic Execution of LBIST STC respectively) on our RM48L952.
In the Software Safety Manual (SPNU592A–April 2015–Revised October 2016) p 17 it can be found that both of these tests have to be performed using the SL_SelfTest_STC function from the API.
The SL_SelfTest_STC function has the following definition:
| boolean SL_SelfTest_STC | ( | register SL_SelfTestType | testType, |
| register boolean | bMode, | ||
| register SL_STC_Config * | config | ||
| ) |
the API documentation shows that testType has 2 valid values (for R4 devices) : STC_RUN and STC_COMPARE_SELFCHECK.
I assume one of these is for CPU2A and the other for CPU2B.
The API documentation also mentions the following:
Note: Function DOES NOT RETURN if STC was started
Note: At the end of the STC execution a CPU reset is issued by the STC controller. So the application startup must ensure that the STC is not-executed when reset type is RESET_TYPE_CPU & when the debugger is connected.
It seems strange that a periodic test causes a reset, is this the way it was intended or am I missing something?