Part Number: TM4C123BE6PZ
Tool/software: TI-RTOS
Hello,
I try to implement a TI-RTOS on a custom board with a TM4C123BE6PZ.
What I do is the following: I take the empty_min Example of the EK-TM4C123GXL from the Resource Explorer. I change the target device to my processor.
Build the project and debug it. As soon the BIOS_Start function is called, the loader_exit() is called. (see the calling trace in the attachment).
I even tried to comment the GPIO Init function and gpiowrite and toggle, so that only the basic things: Create the task and and schedule the task, should work, but with no effort.
The calling trace goes from 0xfffffffc (no symbols are defined) right to Hwi_excHandler.
I use Code composer studio v7. I attached the project, which will go right into the error.
I hope you can give me a hint, what else needs to be changed to get it working, that at least the bios is starting and the task is running.
I'm a little bit desperate, cause I'm trying to get it working now for a week...