This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C1294NCPDT: CMSIS 5.1 DSP Pack

Part Number: TM4C1294NCPDT

Tool/software: TI-RTOS

Hi

I have worked on project decided it time to implement CMSIS FFT. 

I could not find CMSIS being used by TI-RTOS package (as I have used before in NCPxxxx MCU and similar).

I do not want to restart project from strach, how to integrate CMSIS DSP pack into library.

I use base code from USB demo CDC and build upward with many peripheral and RTOS based application code

(I note the simplelink_msp432p4_sdk_2_20_00_12 has FFT code, why CMSIS FFT is not used instead?). 

TivaWare_C_Series-2.1.4.178

tirtos_tivac_2_16_00_08

bios_6_70_01_03

and CCS 8.0