Part Number: LAUNCHXL-TMS57004
Other Parts Discussed in Thread: TMS570LC4357, TMS570LS1224, HALCOGEN, TMS570LS0432
Hello All,
I am developing a Battery management system for Li-ion batteries using Bq76pl455 and TMS57004. In this, I need sample data from bq76pl455 every 1 second and perform BMS task. But I am not able to complete the task in 1 second due to large no. of computations. I am thinking of using a microcontroller with higher RAM and speed. On the product page, I found that TMS570LS1224 and TMS570LC4357 microcontrollers have higher RAM and speed than TMS57004.
So if I generate halcogen files for TMS570LS1224 and TMS570LC4357 then can I use the same CCS code which I have written for TMS57004 in order build a BMS?
Also, do I need to perform some changes in hardware for using TMS570LS1224 and TMS570LC4357?
Regards,
Gunit