Part Number: TM4C1290NCPDT
See original thread: e2e.ti.com/.../471743
This issue still hasn't been fixed in TivaWare_C_Series-2.1.4.178 though the original thread is closed.
I want to use a full width 32 bit timer in periodic mode to toggle a CCP0 pin:
TimerConfigure(TIMER2_BASE, TIMER_CFG_PERIODIC | TIMER_CFG_A_ACT_TOGGLE);
timer.h:
#define TIMER_CFG_PERIODIC 0x00000022 // Full-width periodic timer
#define TIMER_CFG_SPLIT_PAIR 0x04000000 // Two half-width timers
#define TIMER_CFG_A_ACT_TOGGLE 0x00020000 // Timer A compare action toggle.
In TimerConfigure(), the following assert will not allow any other config bit to be set if TIMER_CFG_PERIODIC is selected. It works fine without the assert.
ASSERT(
(ui32Config == TIMER_CFG_ONE_SHOT) ||
(ui32Config == TIMER_CFG_ONE_SHOT_UP) ||
(ui32Config == TIMER_CFG_PERIODIC) ||
(ui32Config == TIMER_CFG_PERIODIC_UP) ||
(ui32Config == TIMER_CFG_RTC) ||
((ui32Config & 0xff000000) == TIMER_CFG_SPLIT_PAIR));
This doesn't look correct. But if it is correct: how is TimerConfigure() supposed to be used to get a full width 32 bit timer in periodic mode to toggle a CCP0 pin?