Part Number: TMDXRM57LHDK
Other Parts Discussed in Thread: HALCOGEN
Hello community,
I am trying to set up 8 PWM signals on N2HET1 and 8 more on N2HET2 using HALCoGen. I am using the Hercules RM57 HDK. The HET1 PWM signals are working as expected but the HET2 ones are not showing up at all (0 voltage at the pins). I saw in this post that there was a HALCoGen bug related to my problem and that the problem was resolved by manually setting one of the HET modules to be the master (changing the contents of GCR). This solution seemed to work for the RM48 HDK. However, I have tried all possible combinations of master/slave with my RM57 HDK and the problem is still there. Does anybody happen to know if this is a known bug and if there is a RM57 workaround for it? Or maybe any possible configuration errors I might have? Any help will be greatly appreciated.
I attached the HALCoGen file I am using in case it helps. The HALCoGen version I have is 4.07.00.
Thanks and Regards,
Surialic