Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL
Hello Everyone,
I am using Tiva C Series evaluation board for the frequency measurement, for this I used a reference timer running on 1 MHz.
System is running on 120 MHz clock, timer source clock is also system clock. Actually I want to figure out the frequency up to ppm level.
My concern is here the reference timer which I am using for frequency measurement, this timer self has error of 0.0025%.
So, can I create a 1 uS timer with 0 ppm accuracy with this board?
Please help on this.
Thanks & Regards
Piyush Purohit