Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: TM4C1294NCZAD, STRIKE, EK-TM4C1294XL
Hi,
I recently had a TM4C1294 Micro-Controller fail catastrophically after 3 months of normal operation. The failure was on a design that is a couple of years old and a failure mode that I have not witnessed previously. The device was pulling down the 3V3 supply line. A resistance measurement from VDD to 0V on the device was less than 1 ohm. We replaced the device on the board. Which now runs as expected. A through inspection of supply voltages an signals associated with the processor yielded no clues as to the root cause of the failure.
I have considered ESD damage, but in the past this generally manifests as FLASH corruption and not catastrophic failure. I also considered CMOS latch up but I believe that this has been eradicated from modern CMOS devices. Assembly/manufacturing issue is another possible cause but our initial inspection of the failed device provided no obvious assembly issues, no shorts etc.
If anyone has any ideas as to possible root causes or has experienced a similar failure mechanism. I would be interested to hear from you.
Thank you.