This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM46L852: Simultaneous use of Ethernet and USB

Part Number: RM46L852

Given the required switch settings (DIP Switch S2) for the Evaluation module (RM46 Hercules Development Kit) for the RM46L852 It appears that it is not possible to simultaneously utilize both Ethernet and USB with the HDK. Is this correct?

 Except for the obvious sharing of pins between USB.1 and MII are there any other resources (such as device memory) within the RM46L852 that are shared between the USB modules and MII that prohibits simultaneous utilization of Ethernet and USB.2 (as Host) by the RM46L852?