Other Parts Discussed in Thread: TMS470R1B768
Hi,
I'm writing a bootloader program for TMS470R1B768, using F05 Flash API to erase and program flash.
After reading SPNU257, I am a little confused about the "Flash Delay Parameter Values".
In the user's specification, a table is provided to determine the Flash Delay Parameter based on "Frequency". My question is what is this frequency, is it SYSCLK or ICLK or something else?
If this is the SYSCLK, is it right that the F05 Flash API support a maximum frequency of 24MHz. Can I erase or program under a higher SYSCLK frequency (like 48MHz).
Thanks in advance.