Dear Sir,
Currently We are using TM4C123GH6PGE DSP for Solar Water Pumping System for 3-Phase AC Induction Motor Control (SV PWM Based) Using V/F technique.
Using this DSP we are successfully producing already 1000 units of 5KW Solar Water Pumping Inverters (VFD Drive) in Market for operating 3-Phase AC Induction Motor.
For this current design, we are sensing Input DC voltage, Input DC current sensing and output AC current senses ( 2 phases) for protections only not for any induction motor control.
Now, We are planning for BLDC/PMSM Motor Operated Drive with same DSP TM4C123GH6PGE. We have few doubts and need some technical information
1. Is this DSP supports this application i.e instead of 3-Phase AC induction Motor, can we use 3-Phase BLDC Motor
2. Is any changes need in my hardware such as Inverter Output Voltage senses, all 3-phases current senses?
3. Any specific algorithms for control 3-Phase BLDC Motor, if there please guide us and provide references based on this DSP
So, kindly support us.
We are awaiting for your support
Regards
Suresh Babu P