On Page 260, PTBOCTL register, VDD_UBOR's reset value is 0x3, or RESET
On Page 224, "If a brown-out condition is detected, the system may generate an interrupt, a system reset or a Power-On Reset. The default value at reset is to generate an interrupt."
I use CCS to look at the register after reset, it seems to agree with the first one, 0x3 or RESET
So the micro will always reset when Vdd is below 2.86 unless we change it, correct?
Thanks for reply!
DC