Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: PCM2903C, TLV320ADC3101
Hi,
i want to use the TM4C1294 to get Audio Data and send it via USB to PC.
Is there a USB Library driver that acts like a USB Soundcard?
At the moment i am using the PCM2903C with MSP432 and have 2x USB to PC.
The PCM2903C is a sound card that has stereo audio with max. 16Bit 48kHz sampling. The MSP432 is used to controll buttons, sensors etc..
I whish i could move to TM4C1294 and replace both ICs in one.
If there is no driver USB for audio codec, then is there a simple example of sending 48kHz 16Bit to a PC like "usb_dev_audio"?
Obs: I would use an external ADC with SPI interface