Part Number: TM4C1294NCPDT
Tool/software: Code Composer Studio
Hello ,
I am just begining of this card software . I have a problem with i2c . I just wanna make sure i2c pin are activated or note . I mean my codes are right or not . I just follow code flow from Using Feature Set of I2C Master on TM4C129x .
My goal is to control i2c pins are working . Thats why I just do step : Configuration of IO’s . My problem is pins are not activated . I just control SCL pin . I need to get clock graph on oscilloscope . But I cant . My code is below ;
Note that : I just wanna check 2 port they are working or not .
#include <stdarg.h>
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_i2c.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "driverlib/i2c.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
/**
* main.c
*/
int main(void)
{
//Enable GPIO for Configuring the I2C Interface Pins
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
//
// Wait for the Peripheral to be ready for programming
//
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOB)
|| !SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOL));
//
// Configure Pins for I2C2 Master Interface
//
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
//
//
GPIOPinConfigure(GPIO_PL1_I2C2SCL);
GPIOPinConfigure(GPIO_PL0_I2C2SDA);
GPIOPinTypeI2C(GPIO_PORTL_BASE, GPIO_PIN_0);
GPIOPinTypeI2CSCL(GPIO_PORTL_BASE, GPIO_PIN_1);
return 0;
}