This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: EPI Host Bus mode setup

Part Number: TM4C1294NCPDT


Hi,

Using the CCS environment are there any code examples of setting up the TM4C1294 External Peripheral Interface (EPI) in

  1. Host Bus 16 bit mode (timing diagram as per data sheet Figures 11-12 and 11-13)
  2. Host Bus 8 bit mode (timing diagram as per data sheet Figures 11-12 and 11-13)
  • I don't have examples for those modes. There is the example for the SDRAM interface in:
    C:\ti\TivaWare_C_Series-2.1.4.178\examples\peripherals\epi
    Also there are several discussions on the forum:
    e2e.ti.com/search
  • Hi
    The following code may help.

    EPIModeSet(EPI0_BASE, EPI_MODE_HB16); //general mode EPI_MODE_GENERAL EPI_MODE_HB16
    EPIDividerSet(EPI0_BASE, 10); //1=60MHz, 10=10MHz, 119=1MHz Sets the clock divider for the EPI module’s CS0n/CS1n.
    EPIConfigHB16Set(EPI0_BASE,
    EPI_HB16_MODE_ADDEMUX | //sets data and address muxed, AD[15:0].
    EPI_HB16_WRWAIT_3 | //sets write wait state to 2 EPI clocks.
    EPI_HB16_RDWAIT_3 | //sets read wait state to 2 EPI clocks.
    EPI_HB16_CLOCK_GATE_IDLE| // holds the EPI clock low when no data is available to read or write.
    EPI_HB16_CSCFG_CS, //sets address latch active low.
    1); // the maximum number of external clocks to wait if a FIFO ready signal is
    //holding off the transaction.

    EPIAddressMapSet(EPI0_BASE,
    EPI_ADDR_PER_SIZE_256MB | //256MB location
    EPI_ADDR_PER_BASE_A); //EPI0 is mapped from 0xA0000000 to 0xA00000FF.

    // Set the EPI memory pointer to the base of EPI memory space. Note that
    // g_pui16EPISdram is declared as volatile so the compiler should not
    // optimize reads out of the memory. With this pointer, the memory space
    // is accessed like a simple array.
    g_pui16EPISdram = (uint16_t *)0xA0000000;

    // READ WRITE OPERARION FOR VERIFICATION
    // A= g_pui16EPISdram[0];

    Regards,
    Digvijay