Part Number: TM4C123BH6ZRB
Hi,
I am having some trouble in figuring out the maximum GPIO current per output pin. I see that there are 2,4,8 mA drive mentioned in the GPIO section but in the electrical characteristics the maximum GPIO current per output pin is defined as 64mA. This maximum current also has a note that says not recommended for extended periods of operation. What would be the maximum current per GPIO pin for extended periods of operation? I would like to know this because I am trying to drive four or five solid state relays from TM4C123xxx or TM4c129xxx whichever is better current drive since both work for the rest of our application.
Thanks!