Other Parts Discussed in Thread: LAUNCHXL-TMS57004, BQ76PL455A-Q1
Hi,
My friends and I are working on a battery management system with which we are trying to use the "Hercules TMS570LS0432 Launchpad ---- LAUNCHXL-TMS57004" and the BMS that we are using is the "BQ76PL455A-Q1" board.
As we searched on the internet, we found that the Texas Instruments documentations suggest that we need to get rid of 2 resistors which are placed on the 38th and 39th pins of the FT2232HL (which is on the board) in order for us to make communication between the 2. But according to this forum one of the user removed only one resistor (R8) which is placed on the 38th pin of the FT2232HL.
We can't understand the purpose for the removal of the resistors to create Uart communication, Also after removing the resistors would we still be able to program and debug the board using the USB connection?
Thanks in advance,
Halid