Part Number: TM4C1294NCPDT
Hello,
Would be possible to connect two CAN controllers together ?
MCU0_CAN_TX->MCU1_CAN_RX
MCU1_CAN_TX->MCU0_CAN_RX
I do not need a bus, therefore I do not need signals translation. It is just for testing.
Thank you,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1294NCPDT
Hello,
Would be possible to connect two CAN controllers together ?
MCU0_CAN_TX->MCU1_CAN_RX
MCU1_CAN_TX->MCU0_CAN_RX
I do not need a bus, therefore I do not need signals translation. It is just for testing.
Thank you,
With 'ALL' risk - fully accepted & acknowledged by (any) user - firm/I have been advised (that the above noted 'TX reflection') (may) be achieved via the insertion of a resistor between CAN_TX and CAN_RX. (~10K seems a 'reasonable' starting point)
Such well qualifies as a, 'Quick and (very) Dirty' implementation. Note that I am not 'advocating for this' - instead simply 'reporting the belief/findings' - of one or more of my firm's clients. This path chosen - only - if/when clients were 'rushed & desperate.' (and for 'test only' - knowledge gleaning - purposes)
Accept too - that 'Any Real World' application 'will demand' use of CAN Transceivers (one at each end) along w/suitable termination. Such xcvrs. are available w/both 5V & 3V3 supply inputs - the latter (3V3) should be employed for MCU's here...
Hello,
Thanks a lot guys.
Your replies solved my issue (actually my doubt).
Thank you,
Good that! However - you have, 'Marked your (own) post - as the one which Resolved your issue."
Yet - your post simply, 'Noted that another, earlier arriving post - had provided the (real) Resolution." It is one - or both - of those earlier posts - which should (now) more correctly receive - your 'This Resolved' Green Stamping (Award)... You 'can' make such award to multiple posts - especially those which (really) Resolved your Issue/Doubt...
BTW - great landscape w/in your avatar. Where are you located? Looks wonderful...
Briceag Cosmin said:It is somehow weird that I have the option to mark my own post as being "solved".
So absolutely true - my friend! Such proves a 'long-standing' forum WEAKNESS - which remains, 'uncorrected.' Even weirder - the (fairly) recent decision to, 'Do AWAY WITH' - the always (motivating) 'LIKE!'
Thank you for your kindness - and - when you've a moment - might you test my clients' (deliberately plural) report of, 'Success via (simple) resistor feedback - between CAN_TX & CAN_RX? That would be appreciated - and may serve (multiple) others here - as well.
Yet - as I past advised - you must deploy (real) CAN-TRANSCEIVERS for 'Real World' applications - and you're urged to move in that direction - sooner rather than later. (As a sailor - the solution 'offered up' was of the, 'Any Port in a Storm' category - and (not all) ports prove friendly...