Part Number: TMS570LS0432
Other Parts Discussed in Thread: HALCOGEN
The initialization sequence of the TMS570LS04x/03x (SPNA163) points to the check of any ESM group3 error, and actually the corresponding source code generated by HALcoGen is:
/* Check if there were ESM group3 errors during power-up.
* These could occur during eFuse auto-load or during reads from flash OTP
* during power-up. Device operation is not reliable and not recommended
* in this case.
* An ESM group3 error only drives the nERROR pin low. An external circuit
* that monitors the nERROR pin must take the appropriate action to ensure that
* the system is placed in a safe state, as determined by the application.
*/
if ((esmREG->SR1[2]) != 0U)
{
/* USER CODE BEGIN (24) */
/* USER CODE END */
/*SAFETYMCUSW 5 C MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
/*SAFETYMCUSW 26 S MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
for(;;)
{
}/* Wait */
/* USER CODE BEGIN (25) */
/* USER CODE END */
}
Nevertheless, the group 3 of ESM is not available for selection in Halcogen. Anyway, it checks the group 2 (!!!) only. Can somebody help me to understand how is checking against ESM error group 3?
Thanks ahead.