Part Number: HERCULES-F021FLASHAPI
Hello,
i am using below listed tools/software in development of flash Erase/program application:
CCS version : 8.0.0
F021 API : 02.01.01
Emulator : XDS100 emulator.
PC OS : Windows 7
below are sequence of steps is used for programming 0x00180000 flash memory:
Fapi_setActiveFlashBank(Fapi_FlashBank1);
Fapi_enableMainBankSectors(0xFFFF);
Fapi_enableEepromBankSectors(0xFFFFFFFF, 0xFFFFFFFF);
Fapi_issueAsyncCommandWithAddress(Fapi_EraseBank,(uint32 *) 0x00180000);
Fapi_issueAsyncCommandWithAddress - autoeccgeneration mode for programming.
i am able to program the memory.
Since i am performing erase/program operation on Bank1, i do not require to enable EEPROM ban sectors so excluded "Fapi_enableEepromBankSectors" line from above mentioned sequence. i am not able see the program data in memory browser. what could be the reason for this?
thanks in advance.
Regards,
Kalyan