Part Number: TMS570LS0714
Tool/software: Code Composer Studio
Dear E2E:
Recently,we found that the result value in ADC1 is a little bigger than in ADC2 when we read voltage from AD module.So I have some problems as following:
(1)There are two ADC module in TMS570LS0714(ADC1 and ADC2).What's the differece between them?
(2)There are two ways to read the result from ADC module.(FIFO and RAM).Under the same conditions, Which way can get the result much faster?
(3)What should we notice, when we use ADC module?
Thanks and Regards,
Yu Chen