Part Number: TMS570LS3137
My system requires 3 interrupts with different frequencies and priorities. I have a 20Khz ISR bound to the FIQ, and a 5Khz ISR is generated via the software-interrupt using the IRQ (and can be preempted by the FIQ). I would like to create a third interrupt running at 100Hz that could be preempted by either the 5Khz or 20Khz interrupts. I think the answer here is no, but I need to be sure because the work-around to this is much work.
Thanks,
Jim