Part Number: TMS570LS0232
Other Parts Discussed in Thread: HALCOGEN
Standard source includes EXTERNL1 in HalCoGen.
But all of Clk Domains are 0 Hz when EXTERNAL1 is selected as the Standard Src.
Can EXTCLKIN be a clock source of GCLK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS0232
Other Parts Discussed in Thread: HALCOGEN
Standard source includes EXTERNL1 in HalCoGen.
But all of Clk Domains are 0 Hz when EXTERNAL1 is selected as the Standard Src.
Can EXTCLKIN be a clock source of GCLK?
Remony,
Does the 30MHz oscillator meet the maximum ViL (0.8V) and minimum ViH (2.0V) specifications of a TTL input signal? The electrical specifications for the external clock input are missing from the TMS570LS0x32 datasheet. We will include these in the next update.
Also, you need to enable the External clock input as a clock source on the "Clk Source" tab in HALCoGen.
Regards,
Sunil
Sunil Oak,
Yes, It does. It supplies 3.3V square wave form.
I enable the external clock input as a clock source on the "Clk Source" tab in HALCoGen.
But "Clk Domains" in HALCoGen are zero.
I don't know why "Clk Domains" aren't apply the External clock
I'm going to change clock pin from the EXTCLKIN to the OSCIN.
The OSCIN has input range from 5MHz to 20MHz. So I need to change frequency of oscillator.
Is it OK?