Part Number: TMS570LS1224
Hello,
I am measuring code using the PMU. The thing I am wondering about is that when i measure my code with the microcontroller at 160MHz the number of clock ticks are greater than when i measure with a lower frequency. Should not the number of clock tick stay the same for the same code?
PS: The code is only pure calculations, and not dependent on any other events
Eirik