Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN,
Tool/software: Code Composer Studio
Hi,
I am trying to use MIBSPI1 and MIBSPI5 modules of TMS570LS1224. I generated driver code with Halcogen but mibSpiInit() function only initialize mibspiREG1 registers. Is it a Halcogen bug or is there a way to do it right.
Halcogen version is: 04.06.00
void mibspiInit(void)
{
uint32 i ;
/* USER CODE BEGIN (2) */
/* USER CODE END */
/** @b initialize @b MIBSPI1 */
/** bring MIBSPI out of reset */
mibspiREG1->GCR0 = 0U;
mibspiREG1->GCR0 = 1U;
/** enable MIBSPI1 multibuffered mode and enable buffer RAM */
mibspiREG1->MIBSPIE = (mibspiREG1->MIBSPIE & 0xFFFFFFFEU) | 1U;
/** MIBSPI1 master mode and clock configuration */
mibspiREG1->GCR1 = (mibspiREG1->GCR1 & 0xFFFFFFFCU) | ((uint32)((uint32)1U << 1U) /* CLOKMOD */
| 1U); /* MASTER */
/** MIBSPI1 enable pin configuration */
mibspiREG1->INT0 = (mibspiREG1->INT0 & 0xFEFFFFFFU) | (uint32)((uint32)0U << 24U); /* ENABLE HIGHZ */
/** - Delays */
mibspiREG1->DELAY = (uint32)((uint32)0U << 24U) /* C2TDELAY */
| (uint32)((uint32)0U << 16U) /* T2CDELAY */
| (uint32)((uint32)0U << 8U) /* T2EDELAY */
| (uint32)((uint32)0U << 0U); /* C2EDELAY */
/** - Data Format 0 */
mibspiREG1->FMT0 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)1U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)15U << 8U) /* baudrate prescale */
| (uint32)((uint32)14U << 0U); /* data word length */
/** - Data Format 1 */
mibspiREG1->FMT1 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)79U << 8U) /* baudrate prescale */
| (uint32)((uint32)16U << 0U); /* data word length */
/** - Data Format 2 */
mibspiREG1->FMT2 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)79U << 8U) /* baudrate prescale */
| (uint32)((uint32)16U << 0U); /* data word length */
/** - Data Format 3 */
mibspiREG1->FMT3 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)79U << 8U) /* baudrate prescale */
| (uint32)((uint32)16U << 0U); /* data word length */
/** - Default Chip Select */
mibspiREG1->DEF = (uint32)(0xFFU);
/** - wait for buffer initialization complete before accessing MibSPI registers */
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
while ((mibspiREG1->FLG & 0x01000000U) != 0U)
{
} /* Wait */
/** enable MIBSPI RAM Parity */
mibspiREG1->UERRCTRL = (mibspiREG1->UERRCTRL & 0xFFFFFFF0U) | (0x00000005U);
/** - initialize transfer groups */
mibspiREG1->TGCTRL[0U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)0U << 8U); /* start buffer */
mibspiREG1->TGCTRL[1U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)1U << 8U); /* start buffer */
mibspiREG1->TGCTRL[2U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(1U+0U) << 8U); /* start buffer */
mibspiREG1->TGCTRL[3U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(1U+0U+0U) << 8U); /* start buffer */
mibspiREG1->TGCTRL[4U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(1U+0U+0U+0U) << 8U); /* start buffer */
mibspiREG1->TGCTRL[5U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(1U+0U+0U+0U+0U) << 8U); /* start buffer */
mibspiREG1->TGCTRL[6U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(1U+0U+0U+0U+0U+0U) << 8U); /* start buffer */
mibspiREG1->TGCTRL[7U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(1U+0U+0U+0U+0U+0U+0U) << 8U); /* start buffer */
mibspiREG1->TGCTRL[8U] = (uint32)(1U+0U+0U+0U+0U+0U+0U+0U) << 8U;
mibspiREG1->LTGPEND = (mibspiREG1->LTGPEND & 0xFFFF00FFU) | (uint32)((uint32)((1U+0U+0U+0U+0U+0U+0U+0U)-1U) << 8U);
/** - initialize buffer ram */
{
i = 0U;
#if (1U > 0U)
{
#if (1U > 1U)
while (i < (1U-1U))
{
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 11U) /* lock transmission */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_0)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_0)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
#if (0U > 0U)
{
#if (0U > 1U)
while (i < ((1U+0U)-1U))
{
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 11U) /* lock transmission */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_1)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_1)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
#if (0U > 0U)
{
#if (0U > 1U)
while (i < ((1U+0U+0U)-1U))
{
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 11U) /* lock transmission */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_2)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_2)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
#if (0U > 0U)
{
#if (0U > 1U)
while (i < ((1U+0U+0U+0U)-1U))
{
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 11U) /* lock transmission */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_3)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_3)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
#if (0U > 0U)
{
#if (0U > 1U)
while (i < ((1U+0U+0U+0U+0U)-1U))
{
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 11U) /* lock transmission */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_4)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_4)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
#if (0U > 0U)
{
#if (0U > 1U)
while (i < ((1U+0U+0U+0U+0U+0U)-1U))
{
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 11U) /* lock transmission */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_5)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_5)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
#if (0U > 0U)
{
#if (0U > 1U)
while (i < ((1U+0U+0U+0U+0U+0U+0U)-1U))
{
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 11U) /* lock transmission */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_6)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_6)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
#if (0U > 0U)
{
#if (0U > 1U)
while (i < ((1U+0U+0U+0U+0U+0U+0U+0U)-1U))
{
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 11U) /* lock transmission */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_7)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
mibspiRAM1->tx[i].control = (uint16)((uint16)4U << 13U) /* buffer mode */
| (uint16)((uint16)0U << 12U) /* chip select hold */
| (uint16)((uint16)0U << 10U) /* enable WDELAY */
| (uint16)((uint16)0U << 8U) /* data format */
/*SAFETYMCUSW 334 S MR:10.5 <APPROVED> "LDRA Tool issue" */
| ((uint16)(~((uint16)0xFFU ^ (uint16)CS_7)) & (uint16)0x00FFU); /* chip select */
i++;
}
#endif
}
/** - set interrupt levels */
mibspiREG1->LVL = (uint32)((uint32)0U << 9U) /* TXINT */
| (uint32)((uint32)0U << 8U) /* RXINT */
| (uint32)((uint32)0U << 6U) /* OVRNINT */
| (uint32)((uint32)0U << 4U) /* BITERR */
| (uint32)((uint32)0U << 3U) /* DESYNC */
| (uint32)((uint32)0U << 2U) /* PARERR */
| (uint32)((uint32)0U << 1U) /* TIMEOUT */
| (uint32)((uint32)0U << 0U); /* DLENERR */
/** - clear any pending interrupts */
mibspiREG1->FLG |= 0xFFFFU;
/** - enable interrupts */
mibspiREG1->INT0 = (mibspiREG1->INT0 & 0xFFFF0000U)
| (uint32)((uint32)0U << 9U) /* TXINT */
| (uint32)((uint32)0U << 8U) /* RXINT */
| (uint32)((uint32)0U << 6U) /* OVRNINT */
| (uint32)((uint32)0U << 4U) /* BITERR */
| (uint32)((uint32)0U << 3U) /* DESYNC */
| (uint32)((uint32)0U << 2U) /* PARERR */
| (uint32)((uint32)0U << 1U) /* TIMEOUT */
| (uint32)((uint32)0U << 0U); /* DLENERR */
/** @b initialize @b MIBSPI1 @b Port */
/** - MIBSPI1 Port output values */
mibspiREG1->PC3 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 1U) /* SCS[1] */
| (uint32)((uint32)1U << 2U) /* SCS[2] */
| (uint32)((uint32)1U << 3U) /* SCS[3] */
| (uint32)((uint32)1U << 4U) /* SCS[4] */
| (uint32)((uint32)1U << 5U) /* SCS[5] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)0U << 9U) /* CLK */
| (uint32)((uint32)0U << 10U) /* SIMO[0] */
| (uint32)((uint32)0U << 11U) /* SOMI[0] */
| (uint32)((uint32)0U << 17U) /* SIMO[1] */
| (uint32)((uint32)0U << 25U); /* SOMI[1] */
/** - MIBSPI1 Port direction */
mibspiREG1->PC1 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 1U) /* SCS[1] */
| (uint32)((uint32)1U << 2U) /* SCS[2] */
| (uint32)((uint32)1U << 3U) /* SCS[3] */
| (uint32)((uint32)1U << 4U) /* SCS[4] */
| (uint32)((uint32)1U << 5U) /* SCS[5] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)1U << 9U) /* CLK */
| (uint32)((uint32)1U << 10U) /* SIMO[0] */
| (uint32)((uint32)0U << 11U) /* SOMI[0] */
| (uint32)((uint32)0U << 17U) /* SIMO[1] */
| (uint32)((uint32)0U << 25U); /* SOMI[1] */
/** - MIBSPI1 Port open drain enable */
mibspiREG1->PC6 = (uint32)((uint32)0U << 0U) /* SCS[0] */
| (uint32)((uint32)0U << 1U) /* SCS[1] */
| (uint32)((uint32)0U << 2U) /* SCS[2] */
| (uint32)((uint32)0U << 3U) /* SCS[3] */
| (uint32)((uint32)0U << 4U) /* SCS[4] */
| (uint32)((uint32)0U << 5U) /* SCS[5] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)0U << 9U) /* CLK */
| (uint32)((uint32)0U << 10U) /* SIMO[0] */
| (uint32)((uint32)0U << 11U) /* SOMI[0] */
| (uint32)((uint32)0U << 17U) /* SIMO[1] */
| (uint32)((uint32)0U << 25U); /* SOMI[1] */
/** - MIBSPI1 Port pullup / pulldown selection */
mibspiREG1->PC8 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 1U) /* SCS[1] */
| (uint32)((uint32)1U << 2U) /* SCS[2] */
| (uint32)((uint32)1U << 3U) /* SCS[3] */
| (uint32)((uint32)1U << 4U) /* SCS[4] */
| (uint32)((uint32)1U << 5U) /* SCS[5] */
| (uint32)((uint32)1U << 8U) /* ENA */
| (uint32)((uint32)1U << 9U) /* CLK */
| (uint32)((uint32)1U << 10U) /* SIMO[0] */
| (uint32)((uint32)1U << 11U) /* SOMI[0] */
| (uint32)((uint32)1U << 17U) /* SIMO[1] */
| (uint32)((uint32)1U << 25U); /* SOMI[1] */
/** - MIBSPI1 Port pullup / pulldown enable*/
mibspiREG1->PC7 = (uint32)((uint32)0U << 0U) /* SCS[0] */
| (uint32)((uint32)0U << 1U) /* SCS[1] */
| (uint32)((uint32)0U << 2U) /* SCS[2] */
| (uint32)((uint32)0U << 3U) /* SCS[3] */
| (uint32)((uint32)0U << 4U) /* SCS[4] */
| (uint32)((uint32)0U << 5U) /* SCS[5] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)0U << 9U) /* CLK */
| (uint32)((uint32)0U << 10U) /* SIMO[0] */
| (uint32)((uint32)0U << 11U) /* SOMI[0] */
| (uint32)((uint32)0U << 17U) /* SIMO[1] */
| (uint32)((uint32)0U << 25U); /* SOMI[1] */
/* MIBSPI1 set all pins to functional */
mibspiREG1->PC0 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)0U << 1U) /* SCS[1] */
| (uint32)((uint32)0U << 2U) /* SCS[2] */
| (uint32)((uint32)0U << 3U) /* SCS[3] */
| (uint32)((uint32)0U << 4U) /* SCS[4] */
| (uint32)((uint32)0U << 5U) /* SCS[5] */
| (uint32)((uint32)1U << 8U) /* ENA */
| (uint32)((uint32)1U << 9U) /* CLK */
| (uint32)((uint32)1U << 10U) /* SIMO[0] */
| (uint32)((uint32)1U << 11U) /* SOMI[0] */
| (uint32)((uint32)1U << 17U) /* SIMO[1] */
| (uint32)((uint32)1U << 25U); /* SOMI[1] */
/** - Finally start MIBSPI1 */
mibspiREG1->GCR1 = (mibspiREG1->GCR1 & 0xFEFFFFFFU) | 0x01000000U;
/* USER CODE BEGIN (3) */
/* USER CODE END */
}