This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C123GH6PM: Using "#define" with only one argument

Part Number: TM4C123GH6PM


Tool/software: Code Composer Studio

Hello,

The following code is copied from the TIVA C Launchpad workshop Lab 14:

#include "stdint.h"
#include "stdbool.h"
#include "inc/hw_memmap.h"
#include "inc/hw_ints.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "sensorlib/hw_isl29023.h"
#include "sensorlib/i2cm_drv.h"
#include "sensorlib/isl29023.h"
#define DEBUG

My question is about the last line (marked in red)
I've never seen #define used in such a way...I'm used to something as follows:
#define DEBUG some_number

Is this a typo ?