Other Parts Discussed in Thread: UNIFLASH
Hello,
I saw on this thread that the TM4C123 doesn't have a unique ID number:
e2e.ti.com/.../471248
But in the spec file I see this paragraph which indicated that there is a unique ID to each MCU.
Register 1: Device Identification 0 (DID0), offset 0x000
This register identifies the version of the microcontroller. Each microcontroller is uniquely identified
by the combined values of the CLASS field in the DID0 register and the PARTNO field in the DID1
register. The MAJOR and MINOR bit fields indicate the die revision number. Combined, the MAJOR
and MINOR bit fields indicate the part revision number.
Did I misunderstood the spec?