Part Number: TM4C1299NCZAD
Tool/software: TI-RTOS
Hi team
We are desing USB composite device for TM4C1299, the usb deviece have CDC*3 and bulk.
I need use high speed for USB PHY using ULPI.
I use TI-RTOS (2.16.01.14).
Using an oscilloscope we can see bit rates of 60MHz.
question:
1. Is TI-RTOS support USB PHY using ULPI ?
2. When I setting TM4C1299 working at 120M and USB setting to 60MHz, TM4C1299 isn't work.
When I setting 60MHz frequence to USB and TM4C1299, TM4C1299 is working.
How can I setting 120Mhz to TM4C and 60MHz to USB ?
3. Can you provite sample code for TI-RTOS's ULPI?
4. Can you provite document for TI-RTOS's ULPI?
BR,
JK