Part Number: TMS570LS1227
Hi,
Using the HET, I would like to generate an interrupt which can trigger on 'x' microsecond depending on the CNT value.
And once the interrupt triggers, I want a function to be called.
Is there an example which can describe how to map the callback function at the trigger of 'x' microsecond interrupt?
I wouldn't be able to use RTI because all the RTI channels are already being used for another functionality.
Thanks.