Part Number: TMS570LS1227
Hi,
1)
I am using HET1 for:
a) Generating PWM output [using HET1 - pin 14]
b) Capturing PWM frequency & duty cycle [using HET1 - pin 15]
When I physically connect the pin 14 and pin 15, the PWM frequency & duty cycle is correctly showing.
However, when I generate another PWM output (from ePWM pin) and connect this to HET1 pin 15 for capture, it is not giving correct PWM frequency and duty cycle.
Is this behavior normal? I am able to successfully observe the PWM values if I connect to PWM output pin to eCAP.
2)
Using the eCAP pin, I am able to successfully observe PWM frequency and duty cycle. However, I am unable to perform Edge capture and PWM frequency/duty cycle capture using the same pin. Is there a software overhead to allow both edge capture & freq/duty capture? I won't be able to use HET for edge capture because all the HET pins are being used for PWM output.
Thanks.