Other Parts Discussed in Thread: HALCOGEN
I am using TMS570 Hercules Dev Kit.
I am fighting with ADC (one channel), data acquisition frequency is determined by RT (e.g. 1-50kHz) and FATfs library for data acquisition (SD card slot). Everything looked fine but than I started tests with sinewaves from generator.... and .... wait where are my samples? ;/
The problem is, every 256 samples (it is constant value and it is independent from acquisition frequency) some samples are missing. I do not have any other interrupts. I checked time of code inside my interrupt and the max value is 7,0us. (rtiGetCurrentTick = 70, with closk 10M).
Here is my example data:
and my code:
if (notification == rtiNOTIFICATION_COMPARE0)
{
/* ADC conversion */
adcStartConversion(adcREG1, adcGROUP1);
while(!adcIsConversionComplete(adcREG1, adcGROUP1));
adcGetData(adcREG1, adcGROUP1, adc_data_ptr); //Store conversion into ADC pointer
value = (uint16_t)((*adc_data_ptr).value);
// Convert uint16_t data into 2x BYTE
dataBufferPtr[0] = (value >> 8) & 0xFF;
dataBufferPtr[1] = value & 0xFF;
/* Write file */
f_write(&fsrc, &dataBuffer, bufferSize, &bw);
bufferFIlledCount = bufferFIlledCount + 1;
dataBufferPtr = &dataBuffer;
/* Check if number of conversion reached number required */
if (bufferFIlledCount == buffersToBeSaved)
{
/* Close the file */
res = f_close(&fsrc);
}
}
Where could be a problem? If it can help I can also add screenshots from my HalCoGen project.