Part Number: TM4C123GH6PM
Greetings,
I was facing an issue when interfacing Lora module RN2483 of microchip over UART communication.
The lux variable when i am directly feeding the data into it its successfully getting transmitted in HEX format while I am trying to transmit fAmbient data which changes upon every sample collected over I2C bus. The which i am receiving on the other end is 0 .
I am pasting the code down below please help.
#include <stdint.h>
#include <string.h>
#include <stdbool.h>
#include <string.h>
#include "inc/hw_memmap.h"
#include "inc/hw_ints.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/adc.h"
#include "driverlib/pin_map.h"
#include "inc/tm4c123gh6pm.h"
#define TARGET_IS_BLIZZARD_RB1
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "sensorlib/hw_isl29023.h"
#include "sensorlib/i2cm_drv.h"
#include "sensorlib/isl29023.h"
#include "driverlib/uart.h"
//functions and variables for setting up the lora network
int sendATCommand(char* ATCommand, char* expected_answer);
void loraConfigure(void);
uint8_t cond;
char luxResult[20] = "";
void stringToHex(char *luxResult);
char packet[25]="radio tx ";
char buffer[50]="";
void concatenate();
float fAmbient;
float lux;
uint32_t ui32ADC0Value[4];
uint32_t ui32ADC3Value[4];
volatile uint32_t ui32TempAvg;
volatile uint32_t ui32TempValueC;
#define DEBUG
#define ISL29023_I2C_ADDRESS 0x44 // ISL29023 I2C address
tI2CMInstance g_sI2CInst; // I2C master driver structure
tISL29023 g_sISL29023Inst; // ISL29023 sensor driver structure
volatile unsigned long g_vui8DataFlag; // Data ready flag
volatile unsigned long g_vui8ErrorFlag; // Error flag
//*************************************************************************
void ISL29023AppCallback(void *pvCallbackData, uint_fast8_t ui8Status)
{
if(ui8Status == I2CM_STATUS_SUCCESS)
{
g_vui8DataFlag = 1;
}
g_vui8ErrorFlag = ui8Status;
}
void ISL29023I2CIntHandler(void)
{
I2CMIntHandler(&g_sI2CInst);
}
void ISL29023AppErrorHandler(char *pcFilename, uint_fast32_t ui32Line)
{
while(1)
{
}
}
void ISL29023AppI2CWait(char *pcFilename, uint_fast32_t ui32Line)
{
while((g_vui8DataFlag == 0) && (g_vui8ErrorFlag == 0));
if(g_vui8ErrorFlag)
{
ISL29023AppErrorHandler(pcFilename, ui32Line);
}
g_vui8DataFlag = 0;
}
int main(void)
{
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
//ADC CONFIGURATION i.e. CPU TEMP
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0); // ENABLE ADC0 MODULE
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE); // ENABLE GPIO for ADC0
GPIOPinTypeADC(GPIO_PORTE_BASE,GPIO_PIN_3|GPIO_PIN_2);// ENABLE A0 AND A1 OF ADC0 MODULE
ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, 2, 0, ADC_CTL_TS | ADC_CTL_IE |
ADC_CTL_END);
ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_CH1 | ADC_CTL_IE |
ADC_CTL_END);
ADCSequenceEnable(ADC0_BASE, 3);
ADCSequenceEnable(ADC0_BASE, 2);
//UART 0
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTConfigSetExpClk(UART0_BASE, SysCtlClockGet(), 57600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_TWO | UART_CONFIG_PAR_NONE));
//UART 1
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinConfigure(GPIO_PB0_U1RX);
GPIOPinConfigure(GPIO_PB1_U1TX);
GPIOPinTypeUART(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTConfigSetExpClk(UART1_BASE, SysCtlClockGet(), 57600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
//loraConfigure();
//I2C CONFIGURATION
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C3);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
GPIOPinConfigure(GPIO_PD0_I2C3SCL);
GPIOPinConfigure(GPIO_PD1_I2C3SDA);
GPIOPinTypeI2CSCL(GPIO_PORTD_BASE, GPIO_PIN_0);
GPIOPinTypeI2C(GPIO_PORTD_BASE, GPIO_PIN_1);
I2CMInit(&g_sI2CInst, I2C3_BASE, INT_I2C3, 0xFF, 0xFF, SysCtlClockGet());
SysCtlDelay(SysCtlClockGet() / 3);
//INITIALISING SENSORS
ISL29023Init(&g_sISL29023Inst, &g_sI2CInst, ISL29023_I2C_ADDRESS,ISL29023AppCallback, &g_sISL29023Inst);
ISL29023AppI2CWait(__FILE__, __LINE__);
ISL29023ReadModifyWrite(&g_sISL29023Inst, ISL29023_O_CMD_I, ISL29023_CMD_I_OP_MODE_M,
ISL29023_CMD_I_OP_MODE_ALS_CONT,
ISL29023AppCallback, &g_sISL29023Inst);
ISL29023AppI2CWait(__FILE__, __LINE__);
while(1)
{
ISL29023DataRead(&g_sISL29023Inst, ISL29023AppCallback, &g_sISL29023Inst);
ISL29023AppI2CWait(__FILE__, __LINE__);
ISL29023DataLightVisibleGetFloat(&g_sISL29023Inst, &fAmbient);
//calculating the CPU temperature
// CLEAR INTERRUPT FLAG FOR ADC0, SEQUENCER 1
ADCIntClear(ADC0_BASE, 1);
// TRIGGER IS GIVEN FOR ADC 0 MODULE, SEQUENCER 1
ADCProcessorTrigger(ADC0_BASE, 1);
// STORE THE CONVERTED VALUE FOR ALL DIFFERENT SAMPLING IN ARRAY
//ui32ADC0Value
ADCSequenceDataGet(ADC0_BASE, 2, ui32ADC0Value);
ui32TempAvg = (ui32ADC0Value[0] + ui32ADC0Value[1] + ui32ADC0Value[2] + ui32ADC0Value[3] + 2)/4;
ui32TempValueC = (1475 - ((2475 * ui32TempAvg)) / 4096)/10;
//calculating decibal values
ADCSequenceDataGet(ADC0_BASE,3,ui32ADC3Value);
//lux=172.607;
//transmiting data via LoRa
sprintf(luxResult, "%g",lux);
stringToHex(luxResult);
concatenate();//creating a packet to be transfered
sendATCommand(packet,"OK\0");
SysCtlDelay(20000000);//500ms delay
sendATCommand("sys reset\r\n\0","OK\0");
lux=fAmbient;
}
}
int sendATCommand(char* ATCommand, char* expected_answer)
{
uint8_t answer=0;
while(*ATCommand!='\0')
{
UARTCharPut(UART1_BASE, *ATCommand);
ATCommand++;
}
SysCtlDelay(4000000);//100 ms delay
while(UARTCharsAvail(UART1_BASE))
{
UARTCharPut(UART0_BASE, UARTCharGet(UART1_BASE));
answer=1;
}
return answer;
}
void loraConfigure(void)
{
cond=sendATCommand("radio set mod lora\r\n\0","OK\0");
SysCtlDelay(400000);//10ms delay
cond=sendATCommand("radio get mod\r\n\0","lora\0");
SysCtlDelay(400000);
cond=sendATCommand("radio set pwr 15\r\n\0","OK\0");
SysCtlDelay(400000);
cond=sendATCommand("radio get pwr\r\n\0","15\0");
SysCtlDelay(400000);
cond=sendATCommand("radio set freq 868100000\r\n\0","OK\0");
SysCtlDelay(400000);
cond=sendATCommand("radio get freq\r\n\0","868100000\0");
SysCtlDelay(400000);
cond=sendATCommand("radio set sf sf12\r\n\0","OK\0");
SysCtlDelay(400000);
cond=sendATCommand("radio get sf\r\n\0","sf12\0");
SysCtlDelay(400000);
cond=sendATCommand("radio set cr 4/5\r\n\0","OK\0");
SysCtlDelay(400000);
cond=sendATCommand("radio get cr\r\n\0","4/5\0");
SysCtlDelay(400000);
cond=sendATCommand("radio set bw 125\r\n\0","OK\0");
SysCtlDelay(400000);
cond=sendATCommand("radio get bw\r\n\0","125\0");
SysCtlDelay(400000);
cond=sendATCommand("radio set crc on\r\n\0","OK\0");
SysCtlDelay(400000);
cond=sendATCommand("radio get crc\r\n\0","on\0");
SysCtlDelay(400000);
}
void stringToHex(char *luxResult)
{
char *pbuffer = buffer;
int i;
int len=strlen( luxResult );
for(i=0;i<len;i++)
{
sprintf(pbuffer, "%x", luxResult[i]);
pbuffer +=2;
}
}
void concatenate()
{
int count=9,i=0;
while(buffer[i]!='\0')
{
packet[count]=buffer[i];
count++;
i++;
}
packet[count++]='\r';
packet[count++]='\n';
}