Part Number: TMS570LS1227
Hi,
I am using TMS570LS1227 in one of the custom board design.
I am interfacing EMIF module with External Asynchronous Memory.
Configuration is
Normal Mode, 16 bit data width.
Currently i am referring section17.2.6.1 in spnu515b and section 17-8.b for the 16-bit data bus normal mode configuration.
Below is the mapping of address lines of Hercules EMIF module with External Asynchronous Memory
| Hercules uC | Ext.Asynchronous Memory |
| BA[1] | A0 |
| A0 | A1 |
| A1 | A2 |
| A2 | A3 |
| A3 | A4 |
| A4 | A5 |
| A5 | A6 |
| A6 | A7 |
| A7 | A8 |
| A8 | A9 |
| A9 | A10 |
| A10 | A11 |
| A11 | A12 |
| BA[0]/A12 | A13 |
I am getting the understanding that BA[0] can be served as EMIF_A[12] . So BA[0] can be connected to A13 of the Asynchronous memory.
I am referring section 17.2.6.1 Interfaces to Asynchronous section. Below is information took from the section.
"Additionally, when the EMIF interfaces to a 16-bit asynchronous device, the EMIF_BA[0] pin can serve as the upper address line EMIF_A[12]."
My question is which line i have to use either BA[0] or A12 to connect the A13 address line of the Asynchronous Memory?
So i am bit confused. So kindly some one suggest on this? So that i can design the custom board accordingly?
Thanks
Chinnasamy.