Part Number: RM48L952
Hello. Are there any limitations or recommendations regarding compatible Micro SD cards that work with the RM48 Hercules Development Kit? I am a bit confused by the different SD card types (SD, SDHC, SDXC, SDUC, UHS, and SD Express), speeds (default speed, high speed, UHS-I, UHS-II, UHS-III, PCIe 3.0), and classes (2, 4, 6, and 10). Or are they all compatible?
Also, is there a working example code that demonstrates use of the RM48 HDK Micro SD slot?
Any details about the HDKs interface would be most welcome.
Thank you for any help!