Part Number: TMS570LS20216
Hello,
My questions are listed below:
1) I want to assign unique serial numbers for my PCBs to avoid possible illegal production. Do these microcontrollers have unique read-only serial numbers or something like this? Probably, a microcontroller from TSM570LS09x/07x series will be selected for new designs. My current idea demands at least one onboard component with unique serial number. In my opinion, it’s not enough to write own serial numbers to FLASH memory. At the moment, I consider an additional IC (for example, DS2411) that stores an unique read-only serial number. However, this solution is more complicated, expensive and perhaps less reliable. What do you recommend?
2) Is it possible to restore source codes from .out files? Protection against unauthorized manufacturing will be realized in code. At the same time, we provide .out files for updating firmware. Therefore, it is imperative that no one can restore source codes from .out files. If so, it is important to disable reading code from chip. Otherwise all efforts will be effectless.
Best regards,
Vitalij Stepin