Part Number: TMS570LS3137
Help,
When trying to use the following api calls within the bootloader uart sample code
Fapi_BlockErase
Fapi_initializeFlashBanks
Fapi_setActiveFlashBank
Fapi_enableMainBankSectors
Fapi_issueAsyncCommandWithAddress
I can single step over the functions, but, when I run over the functions, I end up caught in undef_entry or prefetch_entry.
We are calling Fapi_initializeAPI((Fapi_FmcRegistersType *)F021_CPU0_REGISTER_ADDRESS, (uint32_t)SYS_CLK_FREQ); where SYS_CLK_FREQ == 160 and F021_CPU0_REGISTER_ADDRESS == FFF87000
We are running the F21 and bl_flash from RAM. Any help would be appreciated.
Thanks,
Ron