Part Number: TM4C1294KCPDT
I am using TM4C1294KCPDT Microcontroller. My doubt is can i use uDMA for both UART transmitter and Receiver together. ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1294KCPDT
I am using TM4C1294KCPDT Microcontroller. My doubt is can i use uDMA for both UART transmitter and Receiver together. ?
While technically not simultaneous, the two transactions can happen very close in time. The TX and RX on the UART are very much independent. You can be transmitting and receiving at the same time. Both the transmit and the receive side have FIFOs. The receive FIFO will hold the received data until the uDMA can grab it. Even at the fastest baudrate the uDMA can read a byte received and load another byte to transfer before a second byte can be received.
Bharath Raj said:what if transmitting uDMA data is interpreted as received data by othe uDMA channel?
There are separate request signals for TX and RX that go to different uDMA channels.
Hi Bob,
Thanks for the detailed explanation. I will try with my code and check. Will confirm it if that can be done.