Part Number: TM4C1237E6PM
Hi community,
What is the USB classes supported by TM4C1237E6PM microcontroller ?
Is this micro controller supports CDC Class ?
Thanks & regards,
Divya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1237E6PM
Hi community,
What is the USB classes supported by TM4C1237E6PM microcontroller ?
Is this micro controller supports CDC Class ?
Thanks & regards,
Divya
Hi,
Thanku for clarifying the USB classes on TM4C MCU.
I need some clarification regarding the MCU operating mode & USB functionality.
1)When system does not have any battery (backup supply), then what may be VBAT pin state ? Needs to be shorted with VDDA/VDD ? Hibernate oscillator pins (XOSC0 , XOSC1) ? HIB pin and WAKE pins ?? need to be made as NC ??
Please help me find the solution.
2)As per the TM4C design guidelines VBUS & ID pins are not 5V tolerant at power up and reset state, then how can i build the circuit at power up ?
Thanks & regards,
Divya
Hi,
Thank u for the support.
Still i am having the below queries regarding OTG mode of operation.
what is the input High Voltage level on ID pin ? 3.3V or 5V ?
Thanks & regards,
Divya
Hi ,
Thank for the reply.
Also please help me to find out the answer for the below query.
what is the SPI clock frequency of TM4C1237 micro controller in master mode of operation ?
Thanks & regards,
Divya