This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1231H6PZ: ELEC#05 PIOSC variation, max value over temp

Part Number: TM4C1231H6PZ


In Errata of Rev 7 SPMZ849F there is ELEC#05. The variation of PIOSC is stated as higher than +/- 3%. For a customer application it is needed to understand the max variation over temp of the PIOSC frequency. Pls provide the max data.

The project is urgent!

Thanks!