Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN
Hello forum,
I am validating the clock tree of a TMS570LS3137 implemtation and i want to check the pin clock source valid status.
Therefore I activate the test in the halcogen function mapClocks:
systemREG1->SYSPC1 = 1;
systemREG1->CLKTEST = 0x50101;
I observe the correct PLL Frequency on ECLK Ball, but I cannot interpret the output of the clock valid pin (SEL_GIO_PIN > PLL1 valid status)
+ Q: Is the Pin GIOB[0] (Ball M2)(see section 2.5.1.31; SEL_GIO_PIN Field description of the TRM SPNU499C) or NHET1[12] (Ball B4) (section 2.4.4 of the TRM) the correct terminal to observe?
+ Q: What is the polarity of a valid status? (LOW/HIGH)?
+ Q: Is there a kind of Output Enable necessary to obsere the clock valid status?
regards
Lorenz