Part Number: TM4C1231H6PZ
Hello, I am trying to troubleshooting an issue with one of our boards and determine if it is either the crystal or the micro-controller that is not working. Power is being supplied to the micro-controller and I have another working board to validate issues and compare the crystal signals. The working board has an 8MHz signal and the other board has a low clock signal. If I cannot get a correct clock signal from the crystal, could it be because the micro-controller is not working or is there a way to determine which is the problem?