This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C1294XL: need example code

Part Number: EK-TM4C1294XL

I am working in RTC, but i need to interface with NTP-CLIENT so please some one send me the example of NTP-CLIENT 

thank you

  • Please download the SW-SECURE-IOT-DEMO software package from www.ti.com/.../SW-EK-TM4C129EXL.

    Please also read this post. e2e.ti.com/.../2017227
  • i couldn't get SW-SECURE-IOT-DEMO example in it.. even i download that also. please provide me the example code for that 

    thank you

  • What you download is an installer. You will need to run the installer. Here is the installer.

    spmc022.zip

  • ya i installed same thing but in that not there keil version of code. just there only text files so.

    thank you

  • The example project is only for CCS. This is all we have. You can modify for Keil.
  • i found that code for keil but i could not get call back from UDP. please try solve it
    THANK YOU
  • /**
    * @file
    * SNTP client module
    *
    */


    #include "lwip/opt.h"

    #include "sntp.h"

    #include "lwip/timers.h"
    #include "lwip/udp.h"
    #include "lwip/dns.h"
    #include "lwip/ip_addr.h"
    #include "lwip/pbuf.h"

    #include <string.h>
    #include <time.h>

    extern struct tm RTC;

    uint8_t ntp_send_cmnd_set;

    extern tConfigParameters g_sParameters;

    #if LWIP_UDP

    /** This is simple "SNTP" client for socket or raw API.
    * It is a minimal implementation of SNTPv4 as specified in RFC 4330.
    *
    * For a list of some public NTP servers, see this link :
    * support.ntp.org/.../NTPPoolServers
    *
    * @todo:
    * - set/change servers at runtime
    * - complete SNTP_CHECK_RESPONSE checks 3 and 4
    * - support broadcast/multicast mode?
    */


    #define SNTP_SERVER_DNS 0

    /** Decide whether to build SNTP for socket or raw API
    * The socket API SNTP client is a very minimal implementation that does not
    * fully confor to the SNTPv4 RFC, especially regarding server load and error
    * procesing. */
    #ifndef SNTP_SOCKET
    #define SNTP_SOCKET 0
    #endif

    #if SNTP_SOCKET
    #include "lwip/sockets.h"
    #endif

    /**
    * SNTP_DEBUG: Enable debugging for SNTP.
    */
    #ifndef SNTP_DEBUG
    #define SNTP_DEBUG LWIP_DBG_OFF
    #endif

    /** SNTP server port */
    #ifndef SNTP_PORT
    #define SNTP_PORT 123
    #endif

    /** Set this to 1 to allow SNTP_SERVER_ADDRESS to be a DNS name */
    #ifndef SNTP_SERVER_DNS
    #define SNTP_SERVER_DNS 0
    #endif

    /** Set this to 1 to support more than one server */
    #ifndef SNTP_SUPPORT_MULTIPLE_SERVERS
    #define SNTP_SUPPORT_MULTIPLE_SERVERS 0
    #endif

    /** SNTP server address:
    * - as IPv4 address in "u32_t" format
    * - as a DNS name if SNTP_SERVER_DNS is set to 1
    * May contain multiple server names (e.g. "pool.ntp.org","second.time.server")
    */
    #ifndef SNTP_SERVER_ADDRESS
    #if SNTP_SERVER_DNS
    #define SNTP_SERVER_ADDRESS "pool.ntp.org"
    #else
    #define SNTP_SERVER_ADDRESS "128.138.140.44"
    #endif
    #endif

    /** Sanity check:
    * Define this to
    * - 0 to turn off sanity checks (default; smaller code)
    * - >= 1 to check address and port of the response packet to ensure the
    * response comes from the server we sent the request to.
    * - >= 2 to check returned Originate Timestamp against Transmit Timestamp
    * sent to the server (to ensure response to older request).
    * - >= 3 @todo: discard reply if any of the LI, Stratum, or Transmit Timestamp
    * fields is 0 or the Mode field is not 4 (unicast) or 5 (broadcast).
    * - >= 4 @todo: to check that the Root Delay and Root Dispersion fields are each
    * greater than or equal to 0 and less than infinity, where infinity is
    * currently a cozy number like one second. This check avoids using a
    * server whose synchronization source has expired for a very long time.
    */
    #ifndef SNTP_CHECK_RESPONSE
    #define SNTP_CHECK_RESPONSE 2
    #endif

    /** According to the RFC, this shall be a random delay
    * between 1 and 5 minutes (in milliseconds) to prevent load peaks.
    * This can be defined to a random generation function,
    * which must return the delay in milliseconds as u32_t.
    * Turned off by default.
    */
    #ifndef SNTP_STARTUP_DELAY
    #define SNTP_STARTUP_DELAY 1
    #endif

    /** SNTP receive timeout - in milliseconds
    * Also used as retry timeout - this shouldn't be too low.
    * Default is 3 seconds.
    */
    #ifndef SNTP_RECV_TIMEOUT
    #define SNTP_RECV_TIMEOUT 5000
    #endif

    /** SNTP update delay - in milliseconds
    * Default is 1 hour.
    */
    #ifndef SNTP_UPDATE_DELAY
    #define SNTP_UPDATE_DELAY 900000 //3600000
    #endif
    #if (SNTP_UPDATE_DELAY < 15000) && !SNTP_SUPPRESS_DELAY_CHECK
    #error "SNTPv4 RFC 4330 enforces a minimum update time of 15 seconds!"
    #endif

    /** SNTP macro to change system time and/or the update the RTC clock */
    #ifndef SNTP_SET_SYSTEM_TIME
    #define SNTP_SET_SYSTEM_TIME(sec) ((void)sec)
    #endif

    /** SNTP macro to change system time including microseconds */
    #ifdef SNTP_SET_SYSTEM_TIME_US
    #define SNTP_CALC_TIME_US 1
    #define SNTP_RECEIVE_TIME_SIZE 2
    #else
    #define SNTP_SET_SYSTEM_TIME_US(sec, us)
    #define SNTP_CALC_TIME_US 0
    #define SNTP_RECEIVE_TIME_SIZE 1
    #endif

    /** SNTP macro to get system time, used with SNTP_CHECK_RESPONSE >= 2
    * to send in request and compare in response.
    */
    #ifndef SNTP_GET_SYSTEM_TIME
    #define SNTP_GET_SYSTEM_TIME(sec, us) do { (sec) = 0; (us) = 0; } while(0)
    #endif

    /** Default retry timeout (in milliseconds) if the response
    * received is invalid.
    * This is doubled with each retry until SNTP_RETRY_TIMEOUT_MAX is reached.
    */
    #ifndef SNTP_RETRY_TIMEOUT
    #define SNTP_RETRY_TIMEOUT SNTP_RECV_TIMEOUT
    #endif

    /** Maximum retry timeout (in milliseconds). */
    #ifndef SNTP_RETRY_TIMEOUT_MAX
    #define SNTP_RETRY_TIMEOUT_MAX (SNTP_RETRY_TIMEOUT * 10)
    #endif

    /** Increase retry timeout with every retry sent
    * Default is on to conform to RFC.
    */
    #ifndef SNTP_RETRY_TIMEOUT_EXP
    #define SNTP_RETRY_TIMEOUT_EXP 1
    #endif

    /* the various debug levels for this file */
    #define SNTP_DEBUG_TRACE (SNTP_DEBUG | LWIP_DBG_TRACE)
    #define SNTP_DEBUG_STATE (SNTP_DEBUG | LWIP_DBG_STATE)
    #define SNTP_DEBUG_WARN (SNTP_DEBUG | LWIP_DBG_LEVEL_WARNING)
    #define SNTP_DEBUG_WARN_STATE (SNTP_DEBUG | LWIP_DBG_LEVEL_WARNING | LWIP_DBG_STATE)
    #define SNTP_DEBUG_SERIOUS (SNTP_DEBUG | LWIP_DBG_LEVEL_SERIOUS)

    #define SNTP_ERR_KOD 1

    /* SNTP protocol defines */
    #define SNTP_MSG_LEN 48

    #define SNTP_OFFSET_LI_VN_MODE 0
    #define SNTP_LI_MASK 0xC0
    #define SNTP_LI_NO_WARNING 0x00
    #define SNTP_LI_LAST_MINUTE_61_SEC 0x01
    #define SNTP_LI_LAST_MINUTE_59_SEC 0x02
    #define SNTP_LI_ALARM_CONDITION 0x03 /* (clock not synchronized) */

    #define SNTP_VERSION_MASK 0x38
    #define SNTP_VERSION (4/* NTP Version 4*/<<3)

    #define SNTP_MODE_MASK 0x07
    #define SNTP_MODE_CLIENT 0x03
    #define SNTP_MODE_SERVER 0x04
    #define SNTP_MODE_BROADCAST 0x05

    #define SNTP_OFFSET_STRATUM 1
    #define SNTP_STRATUM_KOD 0x00

    #define SNTP_OFFSET_ORIGINATE_TIME 24
    #define SNTP_OFFSET_RECEIVE_TIME 32
    #define SNTP_OFFSET_TRANSMIT_TIME 40

    /* number of seconds between 1900 and 1970 */
    #define DIFF_SEC_1900_1970 (2208988800UL)

    /**
    * SNTP packet format (without optional fields)
    * Timestamps are coded as 64 bits:
    * - 32 bits seconds since Jan 01, 1970, 00:00
    * - 32 bits seconds fraction (0-padded)
    * For future use, if the MSB in the seconds part is set, seconds are based
    * on Feb 07, 2036, 06:28:16.
    */
    #ifdef PACK_STRUCT_USE_INCLUDES
    # include "arch/bpstruct.h"
    #endif
    PACK_STRUCT_BEGIN
    struct sntp_msg {
    PACK_STRUCT_FIELD(u8_t li_vn_mode);
    PACK_STRUCT_FIELD(u8_t stratum);
    PACK_STRUCT_FIELD(u8_t poll);
    PACK_STRUCT_FIELD(u8_t precision);
    PACK_STRUCT_FIELD(u32_t root_delay);
    PACK_STRUCT_FIELD(u32_t root_dispersion);
    PACK_STRUCT_FIELD(u32_t reference_identifier);
    PACK_STRUCT_FIELD(u32_t reference_timestamp[2]);
    PACK_STRUCT_FIELD(u32_t originate_timestamp[2]);
    PACK_STRUCT_FIELD(u32_t receive_timestamp[2]);
    PACK_STRUCT_FIELD(u32_t transmit_timestamp[2]);
    } PACK_STRUCT_STRUCT;
    PACK_STRUCT_END
    #ifdef PACK_STRUCT_USE_INCLUDES
    # include "arch/epstruct.h"
    #endif




    /* function prototypes */
    static void sntp_request(void *arg);

    /** The UDP pcb used by the SNTP client */
    struct udp_pcb* sntp_pcb;
    /** Addresses of servers */
    static char* sntp_server_addresses[] = {SNTP_SERVER_ADDRESS};
    #if SNTP_SUPPORT_MULTIPLE_SERVERS
    /** The currently used server (initialized to 0) */
    static u8_t sntp_current_server;
    static u8_t sntp_num_servers = sizeof(sntp_server_addresses)/sizeof(char*);
    #else /* SNTP_SUPPORT_MULTIPLE_SERVERS */
    #define sntp_current_server 0
    #endif /* SNTP_SUPPORT_MULTIPLE_SERVERS */

    #if SNTP_RETRY_TIMEOUT_EXP
    #define SNTP_RESET_RETRY_TIMEOUT() sntp_retry_timeout = SNTP_RETRY_TIMEOUT
    /** Retry time, initialized with SNTP_RETRY_TIMEOUT and doubled with each retry. */
    static u32_t sntp_retry_timeout;
    #else /* SNTP_RETRY_TIMEOUT_EXP */
    #define SNTP_RESET_RETRY_TIMEOUT()
    #define sntp_retry_timeout SNTP_RETRY_TIMEOUT
    #endif /* SNTP_RETRY_TIMEOUT_EXP */

    #if SNTP_CHECK_RESPONSE >= 1
    /** Saves the last server address to compare with response */
    static ip_addr_t sntp_last_server_address;
    #endif /* SNTP_CHECK_RESPONSE >= 1 */

    #if SNTP_CHECK_RESPONSE >= 2
    /** Saves the last timestamp sent (which is sent back by the server)
    * to compare against in response */
    static u32_t sntp_last_timestamp_sent[2];
    #endif /* SNTP_CHECK_RESPONSE >= 2 */

    /**
    * SNTP processing of received timestamp
    */
    static void
    sntp_process(u32_t *receive_timestamp)
    {

    /* convert SNTP time (1900-based) to unix GMT time (1970-based)
    * @todo: if MSB is 1, SNTP time is 2036-based!
    */
    time_t t = (ntohl(receive_timestamp[0]) - DIFF_SEC_1900_1970);

    memcpy(&RTC, localtime(&t), sizeof (struct tm));

    HibernateCalendarSet(&RTC);


    UARTprintf("************time_t : %x********************\r\n",t);

    #if SNTP_CALC_TIME_US
    u32_t us = ntohl(receive_timestamp[1]) / 4295;
    SNTP_SET_SYSTEM_TIME_US(t, us);
    /* display local time from GMT time */
    LWIP_DEBUGF(SNTP_DEBUG_TRACE, ("sntp_process: %s, %"U32_F" us", ctime(&t), us));

    #else /* SNTP_CALC_TIME_US */

    /* change system time and/or the update the RTC clock */
    SNTP_SET_SYSTEM_TIME(t);
    /* display local time from GMT time */
    LWIP_DEBUGF(SNTP_DEBUG_TRACE, ("sntp_process: %s", ctime(&t)));
    #endif /* SNTP_CALC_TIME_US */
    }

    /**
    * Initialize request struct to be sent to server.
    */
    void
    sntp_initialize_request(struct sntp_msg *req)
    {
    memset(req, 0, SNTP_MSG_LEN);
    req->li_vn_mode = SNTP_LI_NO_WARNING | SNTP_VERSION | SNTP_MODE_CLIENT;

    #if SNTP_CHECK_RESPONSE >= 2
    {
    u32_t sntp_time_sec, sntp_time_us;
    /* fill in transmit timestamp and save it in 'sntp_last_timestamp_sent' */
    SNTP_GET_SYSTEM_TIME(sntp_time_sec, sntp_time_us);
    sntp_last_timestamp_sent[0] = htonl(sntp_time_sec + DIFF_SEC_1900_1970);
    req->transmit_timestamp[0] = sntp_last_timestamp_sent[0];
    /* we send/save us instead of fraction to be faster... */
    sntp_last_timestamp_sent[1] = htonl(sntp_time_us);
    req->transmit_timestamp[1] = sntp_last_timestamp_sent[1];
    }
    #endif /* SNTP_CHECK_RESPONSE >= 2 */
    }

    #if SNTP_SOCKET

    /**
    * Send an SNTP request via sockets.
    * This is a very minimal implementation that does not fully conform
    * to the SNTPv4 RFC, especially regarding server load and error procesing.
    */
    static void
    sntp_request(void *arg)
    {
    int sock;
    struct sockaddr_in local;
    struct sockaddr_in to;
    int tolen;
    int size;
    int timeout;
    struct sntp_msg sntpmsg;
    ip_addr_t sntp_server_address;

    LWIP_UNUSED_ARG(arg);

    /* if we got a valid SNTP server address... */
    if (ipaddr_aton(SNTP_SERVER_ADDRESS, &sntp_server_address)) {
    /* create new socket */
    sock = lwip_socket(AF_INET, SOCK_DGRAM, 0);
    if (sock >= 0) {
    /* prepare local address */
    memset(&local, 0, sizeof(local));
    local.sin_family = AF_INET;
    local.sin_port = PP_HTONS(INADDR_ANY);
    local.sin_addr.s_addr = PP_HTONL(INADDR_ANY);

    /* bind to local address */
    if (lwip_bind(sock, (struct sockaddr *)&local, sizeof(local)) == 0) {
    /* set recv timeout */
    timeout = SNTP_RECV_TIMEOUT;
    lwip_setsockopt(sock, SOL_SOCKET, SO_RCVTIMEO, (char *)&timeout, sizeof(timeout));

    /* prepare SNTP request */
    sntp_initialize_request(&sntpmsg);

    /* prepare SNTP server address */
    memset(&to, 0, sizeof(to));
    to.sin_family = AF_INET;
    to.sin_port = PP_HTONS(SNTP_PORT);
    inet_addr_from_ipaddr(&to.sin_addr, &sntp_server_address);

    uint32_t ind = 0;

    for(ind = 0;ind < 48 ;ind++)
    UARTprintf("%x ",sntpmsg[ind]);

    /* send SNTP request to server */
    if (lwip_sendto(sock, &sntpmsg, SNTP_MSG_LEN, 0, (struct sockaddr *)&to, sizeof(to)) >= 0) {
    /* receive SNTP server response */
    tolen = sizeof(to);
    size = lwip_recvfrom(sock, &sntpmsg, SNTP_MSG_LEN, 0, (struct sockaddr *)&to, (socklen_t *)&tolen);
    /* if the response size is good */
    if (size == SNTP_MSG_LEN) {
    /* if this is a SNTP response... */
    if (((sntpmsg.li_vn_mode & SNTP_MODE_MASK) == SNTP_MODE_SERVER) ||
    ((sntpmsg.li_vn_mode & SNTP_MODE_MASK) == SNTP_MODE_BROADCAST)) {
    /* do time processing */
    sntp_process(sntpmsg.receive_timestamp);
    } else {
    LWIP_DEBUGF( SNTP_DEBUG_WARN, ("sntp_request: not response frame code\n"));
    }
    }
    } else {
    LWIP_DEBUGF( SNTP_DEBUG_WARN, ("sntp_request: not sendto==%i\n", errno));
    }
    }
    /* close the socket */
    closesocket(sock);
    }
    }
    }



    /**
    * SNTP thread
    */
    static void
    sntp_thread(void *arg)
    {
    LWIP_UNUSED_ARG(arg);
    while(1) {
    sntp_request(NULL);
    sys_msleep(SNTP_UPDATE_DELAY);
    }
    }

    /**
    * Initialize this module when using sockets
    */
    void
    sntp_init(void)
    {
    sys_thread_new("sntp_thread", sntp_thread, NULL, DEFAULT_THREAD_STACKSIZE, DEFAULT_THREAD_PRIO);
    }

    #else /* SNTP_SOCKET */

    /**
    * Retry: send a new request (and increase retry timeout).
    *
    * @param arg is unused (only necessary to conform to sys_timeout)
    */
    static void
    sntp_retry(void* arg)
    {
    LWIP_UNUSED_ARG(arg);

    LWIP_DEBUGF(SNTP_DEBUG_STATE, ("sntp_retry: Next request will be sent in %"U32_F" ms\n",
    sntp_retry_timeout));

    /* set up a timer to send a retry and increase the retry delay */
    sys_timeout(sntp_retry_timeout, sntp_request, NULL);

    #if SNTP_RETRY_TIMEOUT_EXP
    {
    u32_t new_retry_timeout;
    /* increase the timeout for next retry */
    new_retry_timeout = sntp_retry_timeout << 1;
    /* limit to maximum timeout and prevent overflow */
    if ((new_retry_timeout <= SNTP_RETRY_TIMEOUT_MAX) &&
    (new_retry_timeout > sntp_retry_timeout)) {
    sntp_retry_timeout = new_retry_timeout;
    }
    }
    #endif /* SNTP_RETRY_TIMEOUT_EXP */
    }

    #if SNTP_SUPPORT_MULTIPLE_SERVERS
    /**
    * If Kiss-of-Death is received (or another packet parsing error),
    * try the next server or retry the current server and increase the retry
    * timeout if only one server is available.
    *
    * @param arg is unused (only necessary to conform to sys_timeout)
    */
    static void
    sntp_try_next_server(void* arg)
    {
    LWIP_UNUSED_ARG(arg);

    if (sntp_num_servers > 1) {
    /* new server: reset retry timeout */
    SNTP_RESET_RETRY_TIMEOUT();
    sntp_current_server++;
    if (sntp_current_server >= sntp_num_servers) {
    sntp_current_server = 0;
    }
    LWIP_DEBUGF(SNTP_DEBUG_STATE, ("sntp_try_next_server: Sending request to server %"U16_F"\n",
    (u16_t)sntp_current_server));
    /* instantly send a request to the next server */
    sntp_request(NULL);
    } else {
    sntp_retry(NULL);
    }
    }
    #else /* SNTP_SUPPORT_MULTIPLE_SERVERS */
    /* Always retry on error if only one server is supported */
    #define sntp_try_next_server sntp_retry
    #endif /* SNTP_SUPPORT_MULTIPLE_SERVERS */

    /** UDP recv callback for the sntp pcb */
    static void
    sntp_recv(void *arg, struct udp_pcb* pcb, struct pbuf *p, ip_addr_t *addr, u16_t port)
    {
    u8_t mode;
    u8_t stratum;
    u32_t receive_timestamp[SNTP_RECEIVE_TIME_SIZE];
    err_t err;

    LWIP_UNUSED_ARG(arg);
    LWIP_UNUSED_ARG(pcb);

    /* packet received: stop retry timeout */
    sys_untimeout(sntp_try_next_server, NULL);
    sys_untimeout(sntp_request, NULL);

    err = ERR_ARG;
    #if SNTP_CHECK_RESPONSE >= 1
    /* check server address and port */
    if (ip_addr_cmp(addr, &sntp_last_server_address) &&
    (port == SNTP_PORT))
    #else /* SNTP_CHECK_RESPONSE >= 1 */
    LWIP_UNUSED_ARG(addr);
    LWIP_UNUSED_ARG(port);
    #endif /* SNTP_CHECK_RESPONSE >= 1 */
    {
    /* process the response */
    if (p->tot_len == SNTP_MSG_LEN) {
    pbuf_copy_partial(p, &mode, 1, SNTP_OFFSET_LI_VN_MODE);
    mode &= SNTP_MODE_MASK;
    /* if this is a SNTP response... */
    if ((mode == SNTP_MODE_SERVER) ||
    (mode == SNTP_MODE_BROADCAST)) {
    pbuf_copy_partial(p, &stratum, 1, SNTP_OFFSET_STRATUM);
    if (stratum == SNTP_STRATUM_KOD) {
    /* Kiss-of-death packet. Use another server or increase UPDATE_DELAY. */
    err = SNTP_ERR_KOD;
    LWIP_DEBUGF(SNTP_DEBUG_STATE, ("sntp_recv: Received Kiss-of-Death\n"));
    } else {
    #if SNTP_CHECK_RESPONSE >= 2
    /* check originate_timetamp against sntp_last_timestamp_sent */
    u32_t originate_timestamp[2];
    pbuf_copy_partial(p, &originate_timestamp, 8, SNTP_OFFSET_ORIGINATE_TIME);
    if ((originate_timestamp[0] != sntp_last_timestamp_sent[0]) ||
    (originate_timestamp[1] != sntp_last_timestamp_sent[1]))
    {
    LWIP_DEBUGF(SNTP_DEBUG_WARN, ("sntp_recv: Invalid originate timestamp in response\n"));
    } else
    #endif /* SNTP_CHECK_RESPONSE >= 2 */
    /* @todo: add code for SNTP_CHECK_RESPONSE >= 3 and >= 4 here */
    {
    /* correct answer */
    err = ERR_OK;
    pbuf_copy_partial(p, &receive_timestamp, SNTP_RECEIVE_TIME_SIZE * 4, SNTP_OFFSET_RECEIVE_TIME);
    }
    }
    } else {
    LWIP_DEBUGF(SNTP_DEBUG_WARN, ("sntp_recv: Invalid mode in response: %"U16_F"\n", (u16_t)mode));
    }
    } else {
    LWIP_DEBUGF(SNTP_DEBUG_WARN, ("sntp_recv: Invalid packet length: %"U16_F"\n", p->tot_len));
    }
    }
    pbuf_free(p);
    if (err == ERR_OK) {
    /* Correct response, reset retry timeout */
    SNTP_RESET_RETRY_TIMEOUT();

    sntp_process(receive_timestamp);

    /* Set up timeout for next request */
    sys_timeout((u32_t)SNTP_UPDATE_DELAY, sntp_request, NULL);
    LWIP_DEBUGF(SNTP_DEBUG_STATE, ("sntp_recv: Scheduled next time request: %"U32_F" ms\n",
    (u32_t)SNTP_UPDATE_DELAY));
    } else if (err == SNTP_ERR_KOD) {
    /* Kiss-of-death packet. Use another server or increase UPDATE_DELAY. */
    sntp_try_next_server(NULL);
    } else {
    /* another error, try the same server again */
    sntp_retry(NULL);
    }
    }

    /** Actually send an sntp request to a server.
    *
    * @param server_addr resolved IP address of the SNTP server
    */
    static void
    sntp_send_request(ip_addr_t *server_addr)
    {
    struct pbuf* p;
    p = pbuf_alloc(PBUF_TRANSPORT, SNTP_MSG_LEN, PBUF_RAM);
    if (p != NULL) {

    struct sntp_msg *sntpmsg = (struct sntp_msg *)p->payload;

    uint8_t sntp_packet[] = {0x1B,0x00,0x06,0xEC,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x49,0x4E,0x49,0x52,0x00,0x00,0x00,0x00,0x00,0x00,0x00,00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};

    //uint8_t*My_packet = (uint8_t*)p->payload;

    memcpy(p->payload,sntp_packet,48);

    LWIP_DEBUGF(SNTP_DEBUG_STATE, ("sntp_send_request: Sending request to server\n"));
    /* initialize request message */
    //sntp_initialize_request(sntpmsg);



    uint32_t len = 0;
    UARTprintf("PayLoad \r\n");
    // for(len = 0;len < p->len;len++)
    //UARTprintf("%s ",p->payload);
    /* send request */
    UARTprintf("Server Address : %X\r\n",server_addr);
    udp_sendto(sntp_pcb, p, server_addr, SNTP_PORT);
    /* set up receive timeout: try next server or retry on timeout */
    sys_timeout((u32_t)SNTP_RECV_TIMEOUT, sntp_try_next_server, NULL);

    #if SNTP_CHECK_RESPONSE >= 1
    /* save server address to verify it in sntp_recv */
    ip_addr_set(&sntp_last_server_address, server_addr);
    #endif /* SNTP_CHECK_RESPONSE >= 1 */
    } else {
    LWIP_DEBUGF(SNTP_DEBUG_SERIOUS, ("sntp_send_request: Out of memory, trying again in %"U32_F" ms\n",
    (u32_t)SNTP_RETRY_TIMEOUT));
    /* out of memory: set up a timer to send a retry */
    sys_timeout((u32_t)SNTP_RETRY_TIMEOUT, sntp_request, NULL);
    }
    }

    #if SNTP_SERVER_DNS
    /**
    * DNS found callback when using DNS names as server address.
    */
    static void
    sntp_dns_found(const char* hostname, ip_addr_t *ipaddr, void *arg)
    {
    LWIP_UNUSED_ARG(hostname);
    LWIP_UNUSED_ARG(arg);

    if (ipaddr != NULL) {
    /* Address resolved, send request */
    LWIP_DEBUGF(SNTP_DEBUG_STATE, ("sntp_dns_found: Server address resolved, sending request\n"));
    sntp_send_request(ipaddr);
    } else {
    /* DNS resolving failed -> try another server */
    LWIP_DEBUGF(SNTP_DEBUG_WARN_STATE, ("sntp_dns_found: Failed to resolve server address resolved, trying next server\n"));
    sntp_try_next_server(NULL);
    }
    }
    #endif /* SNTP_SERVER_DNS */

    /**
    * Send out an sntp request via raw API.
    *
    * @param arg is unused (only necessary to conform to sys_timeout)
    */
    static void
    sntp_request(void *arg)
    {
    ip_addr_t sntp_server_address;
    err_t err;

    UARTprintf("************Sends Reqst**********\r\n");
    LWIP_UNUSED_ARG(arg);

    /* initialize SNTP server address */
    #if SNTP_SERVER_DNS
    err = dns_gethostbyname((static char*)g_s, &sntp_server_address,
    sntp_dns_found, NULL);


    if (err == ERR_INPROGRESS) {
    /* DNS request sent, wait for sntp_dns_found being called */
    UARTprintf("Dns not resolved\r\n");
    LWIP_DEBUGF(SNTP_DEBUG_STATE, ("sntp_request: Waiting for server address to be resolved.\n"));
    return;
    }
    #else /* SNTP_SERVER_DNS */
    err = ipaddr_aton(g_sParameters.Ntp_Server_IP, &sntp_server_address)
    ? ERR_OK : ERR_ARG;

    #endif /* SNTP_SERVER_DNS */

    if (err == ERR_OK) {

    UARTprintf("*** Send Ntp Reqst ***\r\n");

    sntp_send_request(&sntp_server_address);
    } else {
    /* address conversion failed, try another server */
    LWIP_DEBUGF(SNTP_DEBUG_WARN_STATE, ("sntp_request: Invalid server address, trying next server.\n"));
    sys_timeout((u32_t)SNTP_RETRY_TIMEOUT, sntp_try_next_server, NULL);
    }
    }

    /**
    * Initialize this module when using raw API.
    * Send out request instantly or after SNTP_STARTUP_DELAY.
    */
    void
    sntp_init(void)
    {
    sys_untimeout(sntp_request, NULL);

    SNTP_RESET_RETRY_TIMEOUT();

    sntp_pcb = udp_new();

    UARTprintf("**** SNTP : %x ******\r\n",sntp_pcb);

    if (sntp_pcb != NULL) {
    udp_recv(sntp_pcb, sntp_recv, NULL);
    #if SNTP_STARTUP_DELAY
    sys_timeout(1, sntp_request, NULL);
    #else
    sntp_request(NULL);
    #endif
    }
    }

    #endif /* SNTP_SOCKET */

    #endif /* LWIP_UDP */


    THIS IS MY CODE ..